Loan Calculator Loan Calculator

Loan Amount
Interest Rate
Years
Monthly Payment 1,331
Interest Paid 279,018
Total Paid 479,018

Blogs Blogs

Back

How To Stop Divorce and save Your Marriage?

How to stop divorce is a question that will be relevant both during normal times and during the time when your marriage is in trouble. If you understand the institution of marriage and follow the rules of a sound marriage, the prospect of divorce will never arise. But sometimes, you find that certain developments have taken place which appear to be leading towards a marriage break up, with divorce appearing inevitable. In such a situation, you are naturally concerned with the question how to stop divorce. First thing you should remember is that however grave the situation may appear to be, you can still do a few things to save your marriage. But convince yourself that you don’t want the divorce however bitter things might have developed between you and your spouse.

Here are a few suggestions to stop Divorce

1) Make yourself a more agreeable person: I am not suggesting for a moment that that you have not been conducting yourself in an agreeable way. You may have been conducting yourself in an exemplary way. But a little self examination is not going to hurt. On the other hand, it may do you a lot of good. Your thought process should run like this: ‘There are certain things about me which my spouse doesn’t seem to like. (Otherwise, why should the question of divorce arise at all?) Can I think of the things which he doesn’t like about me and do something about them?’ When you adopt this approach, you will find to your surprise that you are able to zero in on a couple of things about you that you can change for the better. And once you do this, you will find a dramatic improvement in your spouse’s attitude towards you. Please note that I am not asking you to give up your individuality and surrender to the whims of your spouse. All that is required are a few changes which you will not mind implementing. The chances are you will like the changes yourself!

2) Don’t react sharply to your spouse’s proposal for divorce: You can’t stop divorce by angrily dismissing the idea. Your spouse may be expecting you to react violently to the idea so that it will lead to an altercation and culminate in a situation warranting divorce. React cautiously. Say you will think about it. Once you are able to prevent an immediate flare up, you can eventually drop hints that you can still make up, stop divorce and save your marriage.

3) Do not make the mistake of taking your partner for granted: One thing that is universally disliked is being taken for granted. If you are concerned with how to stop divorce, then you should be careful in dealing with your spouse. Don’t dismiss their views or suggestions lightly. If you disagree with your spouse, do it agreeably. Acknowledge the merit of their views and then say that you have a different view. If you want to bring your spouse around to accepting your stand, do it gently. If there is resistance, leave it for the moment. A calm and judicious handling of the differences will ensure that you both will learn to respect each other’s views.

How to stop divorce will no longer be a haunting question.

Next
Comments
  • Peace gold